Part Number: LM5163-Q1
Other Parts Discussed in Thread: LMR38010-Q1,
Good morning
What is the maximum input leakage @150°C (or 125°C) of PGOOD port
(i.e. when voltage is regulated inside of the ‘good’ range,
it should be a MOS --> Zero Gate Voltage Drain Current)
for:
- LMR38010-Q1
- LM5163-Q1
@Vds = 5V - 10V
Do you have any data or graph showing this aspect?
If you don’t have any,
can you suggest similar discrete MOSFETs to draw data from?
Thank you very much in advance
Best regards