This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR51450: I cannot design a circuit for an output other than 5V on WEBENCH.

Part Number: LMR51450

I am trying to build a circuit where I will get 22.V at the input and 12V 5A at the output using LMR51450. The circuit I built by reading the datasheet is attached. I want to compare the circuit I built on Webench, but it automatically accepts the output voltage as 5V and when I set it to 12V, I get a design update failed error.