Hello TI team,
We have a design with 11 power rails sequenced by the UCD90124A and with a main power enable/disable signal coming from a MCU connected to the PMBUS_CNTRL pin.
Now, we would like to have a different variant of the same design where two power rails in the middle of the current power sequence will be missing (the PSUs and the powered components will be physically removed).
Our question is if it is possible to support both variants with the same UCD90124A configuration?
We have an additional (currently unused) GPIO signal between the MCU and the GPI 1 pin of the sequencer. The MCU can set that pin to a state indicating the variant of the board before it toggles the PMBUS_CNTRL signal.
Is it possible to use the Pin Selected Rail States feature together with the PMBUS_CNTRL pin to achieve the following operation?
PMBUS_CNTRL pin | GPI 1 pin | State of the power rails |
LOW | X | All rails are OFF |
HIGH | LOW | All rails are ON |
HIGH | HIGH | All rails are ON, except for two rails in the middle of the sequence (Those two rails should be ignored during the on-/off-sequence) |
Thanks for any help in advance.