Hello,
Regarding the open wire diagnostic of the SRN/SRP channels. If I turn on the OW Sink on SRN/SRP DIAG_COMP_CTRL3. OW_SNK[1:0] = 11, I expect the measured voltage to change in case of an open wire.
If I try this out on a open SRN/SRP connection the measured change of volatge is in the range of ~2mV. Where as the maximal clamped voltage between the pins according to the bq79631 datasheet is 0.9V. (no minimum is sepecified).
Is there any information regarding the minimal/average clamped voltage or the strength of the voltage source for open wire detection on SRN/SRP available?
Regards Josef