This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65263: TPS65263

Part Number: TPS65263

Hi Ti team,

I have a question about TPS65263,  Two of the three output voltages of TPS65263 are not correct.    

power input : 12V

VOUT-1:  1V8 , but I get 1.36V

VOUT-2 : 1V2    1.199V, it is ok

VOUT-3 : 5V   only get 2.375V

could you please help me? thank you so much.

Best Regards

Jill