Part Number: LM3463
Hi,
I would like to know if it is possible to drive 4 independent high power LED (3.3V / 3A) with a the LM3462 and a FET Stage.
I would like to drive the led with a 12 V Power.
On the evaluation board there is 150V/29A Fet but the board can only deliver 200ma per channel,
Is it possible to modify the evaluation board to make my tests ?
Thanks for you help.