Hi team, I have three questions.
1. There is an instruction to connect IGND and REF GND to Chasis (PE).
In this case, it need to connect the 12V output of the secondary side with PELV connection to VDD.
What should I do if I only have SELV output and no PELV output?
2. I think the specification is to use a sense/injection capacitor to provide insulation between the primary and secondary, is that correct?
3. Should the connection between IGND and PE be made from the PE closest to the AC input (near the Y connector)?
Best Regards,