This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2597: TPS25970A design review

Part Number: TPS2597

Hi Team,

Please help to review the schematics.

Thanks.

2100.EFUSE.pdf

  • Hello Peter,

    The schematic in general looks fine but I have noticed few things.

    • ILIM resistor (11K_F2): I am assuming it to be 1.1K resistor based on ILIM calculations.
    • There is no transient protection. We recommend using some decoupling capacitor (very near the input pin in layout) and a TVS diode for input side transient protection and Schotkey diode at the output side. Events like hot plug and output short causes transients which can very easily exceed the absolute maximum of the device. 

    Reply here for any follow up question. If this answers your query, click resolved. 

    Best Regards,
    Arush