Other Parts Discussed in Thread: TPS63024
hello we use a current limiter (250ma) to charge a large cap (3mF) to 5v and then use the TPS630242 to make 3.3v out of it. we choose the buckboost so we can catch large current spikes / make use of more of the large capacitance (from 5v down to 2.5v)
we now got an instability where all energy seems to be "burned" when the output is loaded with 16.5 ohm: the max current (250ma) is drawn on the 5v input (by the limiter) but the cap is only charged up to about 2v. the output is only 2.5v average (and oscillating, vp-p about 1 v). so we got 5v x 0.25a = 1.25w going in and only get 2.5v x 0.15a = 0.38w out.
when loaded with only 33ohm we get a nice stable system with > 90% efficiency
two questions:
- what is causing this instability / burning up all energy? is it the "Output capacitor discharge function" kicking in all the time?
- if i start by loading the output with 33 ohm and later, after the big cap is "full", switch to 16.5 ohm (adding another 33ohm resister in parallel) it works fine. can i delay the "enable" of the buckboost by 100ms?
thanks
frank