Part Number: TPS61088-Q1
Hello team,
my customer has questions for TPS61088-Q1 (RHL0020A).
1. How long is a. in millimeters?
2. is b. (0.2) max value or typ valu?

best regards,
kazusa suzuki
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS61088-Q1
Hello team,
my customer has questions for TPS61088-Q1 (RHL0020A).
1. How long is a. in millimeters?
2. is b. (0.2) max value or typ valu?

best regards,
kazusa suzuki
hello,
thanks. but, for a, package size is 4.5mm *3.5mm. 20mm should be wrong.
could you please check again?
Hi Kazusa,
Sorry, I made a mistake.
the size should be 0.3mm to 0.5mm, 20 means there is 20 of such pads, including horizontal and vertical ones.
Best Regards,
Fergus
Hi Kazusa,
I will further inquire our colleges about this question.
I will reply a soon as I get the result.
Regards,
Fergus
for pin, typ is 0.24mm and i can understand max is 0.29mm.
but, for b. typ is 0.2mm. could you please clarify 0.29 is for b.?
Hi Kazusa,
I will forward to our PE to answer your questions.
Regards,
Fergus