Other Parts Discussed in Thread: BQ27427, BQ27426
Hi,
I want to charge the battery which is having internal cut-off like 3.0 V. below 3.0V there is no output voltage and it is showing 0V from battery so I need to generate a pulse to take it out from its cut off voltage so it can start charged. If battery voltage is not less than its cut-off, it is charging as per configuration. What configuration should be done in bq25619e to take out battery from its cut-off and start the charging normally?
Thanks
Ravi Gohel