This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP55231: Ratiometric

Part Number: LP55231
Other Parts Discussed in Thread: LP5569

Hello,

I am using 2 chips with independent programs and both synced with Trigger line and using the same Clock. I have a problem when using the Ratiometric configuration inside the Engines. I lack some documentation from this part.

Is it possible to explain how to use the Ratiometric inside an Engine? Do I have to add additional Wait orders between lines? Is there an example you can provide using the Ratiometric while fading LEDs in an engine?

Is it possible to change between colors while fading into an Engine? What are the limits of these Engines?

Thank you very much