This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2400: Recommendation for overvoltage protection

Part Number: TPS2400
Other Parts Discussed in Thread: LM74502

Hello,
I have a system that works in the 10-36V range. I want the system to shut down when a voltage above 36V reaches the input of this system. The high voltage coming to the input will vary between 37-100V.
Can you recommend a product that meets these features?