Other Parts Discussed in Thread: TLV61070A, TLV61048
Hi, this is volkan
Greetings from Istanbul.
In my application I need these two fixed DC differential voltage sources to pass the rail to rail level in an opamped circuit where I will drive peak to peak +-5V DC
In order to supply these fixed differential 5V5 DC Supply which I need to feed for the op amp, i am looking for to design Boost/SEPIC Conversions design with Effective, simple and cost friendly way.
I wonder if I can get a total supply of 400ma for +-5,5V and 200ma for -5,5V from single 3V3 DC source with this single simple switcher ? If yes could you please guide me how to i do that ?
I would appreciate if have any examples, design notes or calculation formulas.
If i can not able to get these differential source from single 3v3 then which component is suitable to my application ?
Thank you for the support.
Best Regards
Volkan