This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25618E: BQ25618E Surge voltage

Part Number: BQ25618E

Hi ti team,

What is the maximum surge voltage that BQ25618E can withstand?

  • Hello,

    22 V is the ABS MAX rating for the VAC/VBUS. Please check Section 8.1 on the datasheet for more information. Please note however, that "Stresses beyond those listed under Absolute Maximum Rating may cause permanent damage to the device. These are stress ratings only, which do not imply functional operation of the device at these or any other conditions beyond those indicated under Recommended Operating Condition. Exposure to absolute-maximum-rated conditions for extended periods may affect device reliability."

    Regards,

    Mike Emanuel