Other Parts Discussed in Thread: UCC21732-Q1
We are using the UQQ15241-Q1 and UCC21732-Q1 in an IGBT Gate Driver application (six channels).
We have a stable input voltage of 24.75V (for 1second) before we switch the ENA pins on the UCC15241 high. Typically only half of the six UCC15241 converters start up correctly and pull the PG pin low.
The VDD-VEE voltage is 23.0V (-8/+15V)
To get all channels to start up we have to toggle the ENA pins a severla times within a 0.3 sec.
Is there a limit to how much VDD-VEE Capacitance is safe to use to ensure good startup.
We have 3*10uF plus 0.1uF total at 0V bias which is ~15.1uF at the final 23.0V target voltage.
There is also some VDD-COM and COM-VEE capacitance (12.4uF and 23.2uF at operating bias voltage).
We used the Excel UCC15241 Calculator sheet for the design.
When the converters do start up the rise time is about 6ms to 23V which is well within the soft startup time.
Do we have too much capacitance or is there another issue that causes startup problems?
Regards
Scott