Other Parts Discussed in Thread: , LMG2100R044
TI support good morning
i plan to work with the LMG5200MOFT and have some questions.
1. VCC maximum current is 5mA, why evaluation board LMG5200EVM-02 has 1A LDO? can i use 50mA LDO?
2. do you have similar part in H bridge configuration?
3. can you recommend a driver ( half bridge and full bride) for the input signals instead of the logic with 2 invertor and diode?
(need to include dead time control and enable).
4. notice that VCC (5v) has 5 capacitors, not according to part data sheet .
do I need so many capacitors?
also notice that LDO input has 4 capacitors (again not according to LDO data sheet)
total capacitors 9, is it require? or just good practice?
5. can i drive the LDO voltage from the bridge source? or noise from the bridge might affect LDO output?
6. if 2 half bridge generating H bridge, can i drive both (5v) with single LDO ( 2-3 capacitor near each LMG5200MOFT pin and LDO between parts)?
Yehoram