Hi,
Does LM5035C possible to fulfill below application? Anything reference design can share to us? thank you!
Vin DC24V(18-28V)
VOUT DC48~65V 3.4A
Jeff
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Yes, LM5035C can meet the specs. There is an EVM available but I cannot find any reference design of this device similar to your specs.
Hollo~
Help provide circuit diagrams and transformer specifications (core,Bobbin,wire diameter, coil ratio, inductance) according to our company's needs
Isolated DC To DC SPEC: Vin:DC24V(18-28V) ,Vout:48- 65V/ 3.4A +/-3% , Efficiency:>90 %
Hi,
You can refer to the EVM but design to meet your specs. It is basically to design a half bridge converter which you can search the internet or find design steps from college text book. You need to design yourself. The example is the EVM.