This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCR010505U DC-DC



Hello,

During production test, 10% of DCR010505U DC-DC need input power recyling to restart after we applied a 5 second duration short circuit on its output. Is it an normal operation of the DC-DC (no indication of power recycling needed on the datasheet)? Do we have to warry about the long term reliability of the unit that did not restart without power recycling?

 

 

  • Pierre:

    I reviewed the e-mail concerning power recycling when the output is shorted on 10% of the units.This appears to be the  5V   input power source  is driven into current limit.during the short test.

    The can send my your contact information to my email address.

    I can call you and discuss thsi question.

    tguerin@ti.com

    Tom