Hello,
I'm currently trying to light up a LED (L0-CS0) (150060AS75000 from wurth) with the LP5864 to validate a circuit.
But i currently get no results.
I did try to find some example code for C, but could not find any.
I'm trying to run it in mode 1, VIO_EN is connected to 3v3 and Vsync is connected to a microcontroller and VCC & VLED =3V3
currently I'm doing the flowing:
- reading Dev_config3 to validate the i2c connection.
- write and read 0x01 to Chip_en.
- write and read 0x20 to Dev_initial.
- write and read 0x4D to Dev_config3.
- write and read 0xFF to DC0 (dev.adr:0xA9 mem.adr:0x00)
- write and read 0x7F to pwm_bri0(dev.adr:0xAA mem.adr:0x00)
when measuring SW0 and CS0 I get the following result:
could you help my with this problem?