This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28950: 48V to 10~120V Adjustable output voltage.

Part Number: UCC28950
Other Parts Discussed in Thread: LM5045

Hi professional team.

I'm testing output voltage adjustable power supply.

Maximum  Power : 480[w]   (Burst operating)

Input : 48V.

Output Voltage : 10~120Vdc Adjustable by DAC voltage.

                           Non-isolation type.

Output currnet : max 4A.

Auxiliary voltage : 12V.

controller : UCC28950.

Main Transformer turn ratio : 1-3  (Primary : 7, Secondary : 20 Turns)

- Snubber cap : 470pF, 560R

Efficiency : Don't care.

Unfortunately, UCC28950 controller can adjustable output voltage,

But secondary large spike voltage(Up to 500Vdc) makes me difficult.

Snubber resistor has very lot so it makes smoke in output low voltage.

I read that UCC28950 is not efficiency about low voltage input in other column.

Can you give me another solution more simple?

Ss LM5045  simple solution for me?