Other Parts Discussed in Thread: TL431
Hi Experts,
In LM5155 application note SNVA866A, what's the purpose of Rcomp and Ccomp which are connected Vcomp?
If it's for compensation purpose, how it contribute to Zero and Pole?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Thank you for using the E2E forum.
The main compensation of an isolated flyback is done on the secondary side at the TL431 voltage reference. However, in some cases, RCOMP and CCOMP on the primary side are also needed. RLED is responsible for the mid band gain (AVM). If the needed value for RLED is higher than the maximum possible RLED (depending on the optocoupler, Vout and the voltage reference), RCOMP (on primary side) has to be used. CCOMP on the primary side influences the high frequency pole, as it is in parallel to Copto.
Please note, that the values for Rcomp and Ccomp on the primary side dont have to be the same like Rcomp and Ccomp on the secondary side. They are independed from each other.
For detailed explanation and formulas i recommend the following video: https://www.ti.com/video/5426178629001
Also the following document might be useful for understanding the flyback powerstage and the isolated feedback via optocoupler: https://www.ti.com/seclit/ml/slup340/slup340.pdf
If you have further questions, please feel free to ask.
Best regards,
Moritz