Other Parts Discussed in Thread: LMG3522EVM-042, PMP23338
Hello,
Why are the capacitors C52 and C53 not connected in the layout files of PMP23069?
Regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Why are the capacitors C52 and C53 not connected in the layout files of PMP23069?
Regards,
Hello, C52 and C53 are on bottom layer
Hello Bosheng,
I have attached the screenshot of bottom layer planes
There seem to be a small isolation breaking the planes(rats can be seen as well):


If this is intentional, why are the C52 & C53 connections kept as optional?
Regards,
A GaN daughter is soldered in position 1, the daughter card already have caps for the same purpose of C52 and C53. Position 2 is reserved for a different GaN daughter card, if it is used, then the isolation gap must be shorted. Only position 1 is used in the released PMP23069 board.

Got confused with position 2 as testpoints (as mentioned in the schematic)

So no need to place C52 & C53 on the Mainboard(while using GaN card at position 1) Thanks for the clarification.
May I know which GaN card is compatible for position 2?
Regards,
Hello,
Is there a C2000 card option where the card fits inside the power supply region? (within 68.1mm)
Regards,
I am talking about the mentioned width of the board

Is there a C2000 daughter card option that can be placed directly near J1 & J2?
Regards,
you will need to design your own control card to plug in J1&J2 directly. You can also check PMP23338, it is a similar design, the C2000 control card is plugged in directly.