Other Parts Discussed in Thread: TVS0500
Hi
I selected the TPS78533QKVURQ1 (LDO TPS785-Q1 fixed 3.3V out) for a design for the purpose of converting the 5V coming from a USB connector's VBUS to 3.3V.
Now, I need to add ESD/Transient voltage protection to the VBUS. The datasheet of the LDO states in the absolute maximum section that the maximum input is 6.5V. From this, I believe that I need to find a TVS with a working voltage of 5V and a clamping voltage between 5.5V and 6.5V. Finding one is proving difficult.
The TVS0500 is recommended in ESD and Surge Protection for USB Interfaces section 8.2: VBUS protection. However, its clamping voltage is higher than the absolute maximum input voltage of the LDO.
As to my question: would the TVS0500 be a suitable pairing for this LDO? If not, does TI offer a solution for ESD/transient voltage protection that would fit this LDO. A requirement is minimum (not maximum) pitch of of 0.5mm to make hand soldering feasible for prototyping purposes.
Best regards,
Matthias