Hi ,
We are going to Use this TPS259482AYWP E fuse in our design. The E fuse is connected with J3 Connector from SMPS Part No: (CUS60M)
12 V output from Switched mode power supply (SMPS) that connected with 7A load. Below I attached the SMPS electrical Specification.
1. Above mentioned SMPS output(12V) is connected to the input side of E-fuse. I need to know the E-fuse will not get damage when using this SMPS(CUS60M-12).
2. As per the datasheet , we calculated for a) Slew Rate b)Inrush current c)DV/DT d) ITIMER values .Verify the values are correct or not.
3. Need clarification about the output capacitor, 200uF is enough or else I need to change with lower values.
Thanks in Advance!