Part Number: TPS6594EVM
I am experiencing difficulties connecting the TPS65941111EVM with the "Scalable PMICs GUI 3.0.0" on my Windows system. I am using the offline version for Windows with gcruntime 11. Upon plugging in the USB cable, I observe two new COM devices in the Device Manager and one unrecognized "Virtual COM port" without a driver. When I have the "Device Settings" window open in the GUI, this is the output I receive in the console:


COM4 and COM6 are consistently present on my PC. It appears that the software attempts to connect with COM4, but COM7 is actually the correct port. Although I managed to connect a few times previously, I am unable to do so again.
On a Linux virtual box machine, I encounter an error stating "Controller is not responding," although this is likely due to the virtual machine environment. Below I attached a screenshot of the console and the error message.

The only physical alteration on EVM I have made is connecting V3V3 to VSYS on J15. Power is solely supplied through USB.