Hello,
I'm considering using a TLC59108F device for driving leds. I need to use it as ON/OFF driver, and I've seen this driver was using 2 separates PWM signals to set brightness and dimming. Therefore, for my ON/OFF application, I need to ensure that this ON/OFF is not performed by PWM signal (considering a 99,6% duty cycle is ON), but with a permanent signal to force the output driver to be continiously ON or OFF. Could you confirm that programming the LEDOUT0 & LEDOUT1 registers with "0x00" and "0x01" values gives a continious and permanent OFF or ON output?
Best regards,
Rémi