开关频率异常!
什么原因?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
There may be different reasons but I do not yet have enough info to tell at this moment. I saw your scope picture above. Could you also zoom in the the SW signal so I can see it over smaller time scale, like 1us/div, 50us/div, and 500us/div? Could you also add VIN, SS and 5Vout signals on the same scope picture? I also need to know your transformer datasheet.
Best Regards,
Youhao
Then, lets debug this way: can you remove D25, and see if you have output voltage at the +5V rail? Then install D25 but remove D26, and check the 17V output rail? When doing this, please capture SW and the secondary winding voltage.
Thanks,
Youhao