Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61377EVM: Extend the input range 9V to 16V

Part Number: TPS61377EVM

Hi,

As the TPS61377EVM user guide, the input voltage range is 9V to 16V, but the IC and input caps are rating over 20V, may I use 19V for input?

Suppose it is okay, just double check.

Thanks and Best regards,

Tiger

  • Hi Tiger,

    The EVM can work when input is 19V.

    "The input voltage range is 9V to 16V" refers that the default components on EVM are optimized for this Vin range. Usually it can work also out of this range (still in the device's work range).

    Regards

    Lei