Part Number: TPSI3050
We are a Thyristor manufacturer and we are looking to use the TPSI3050 in one of our reference designs for customers to use in the home appliance sector.
I noticed the driver doesn't make any claims for continuous DC output current, only peak values, which are more applicable to Mosfet's than SCR's. In one of our applications we have a need to use continuous DC gate drive for these devices, with 50mA being commonly applied.
We are likelly to be using the 3 wire mode with a 5V supply. Do you have any data you can share on the output capabilities of the driver under this situation?
Thanks