Other Parts Discussed in Thread: BQSTUDIO
Our new Battery Management Studio EVM won't pass Quick Start.
It starts up with the EVM connected and can communicate with the device (7695_0_36). Initially the pack voltage (23mV) is dramatically lower than the stack (4781mV). Both DSG_FET and CHG_FET are on. The CUV bit is set. OTOH when I click on FET_ENABLE the pack voltage goes up (5083mV) and DSG_FET goes off. When I drop the supply voltage from 48V to 38V nothing changes.
What's up?