HI,
We have made a custom board with LV2862 with 33uH inductor and DLFS1100 etc. We have device heating up badly and goes to thermal shut down.
If we power the device with 24V (output is 12V) it works well but still heats to around 45 degrees (external infrared reading).
If we raise the input to 40V or 42V the device goes to thermal shut down!!
Is this device recommended for 12V 500mA application with 32 to 42V input (10S cells)
Below is the layout and schematics
kind regards
VG