Hi,
I'm seeking assistance in troubleshooting an issue with the TPS63900EVM. I've measured all the resistor values across CFG1-3, and they match the values listed in Table 7-2 and 7-3. However, upon connecting the supply, I'm not receiving any output values.
The setup for JP1 is configured for Vo2, and CFG3 S3.1 is set to high to prevent floating. Similarly, when JP2 is set to Vo1, CFG1 S1.1 and CFG2 S2.1 are set to high. Initially, I managed to obtain output readings, but upon setting switches 6, 7, and 8 to high, the output voltage decreased below the desired level, as shown in the table below. Subsequently, upon repeating the measurements, I'm not obtaining any output at all.
I kindly request assistance in debugging this issue. Thank you in advance for your help.