Other Parts Discussed in Thread: BQ25170EVM, BQ27427, GPCCHEM, BQSTUDIO
Hello,
I am doing a learning cycle to a Li-ion battery with the aid of the BQ27427EVM. This battery has a capacity of 250mAh, a nominal voltage of 3.7V and a charge voltage of 4.2V. However, when I am doing the learning cycle, I can't pass from the charge state to the relaxed one. As you can see in the image below, the learning cycle stays in the charge state even with a battery voltage above 4.2V. Should I do anything else to continue the learning cycle?
Before starting the learning cycle, I programmed the correct chemistry ID (1202 in this case). To charge the battery, I am using the BQ25170EVM with a 4.2V configuration (R5) and a maximum current of 100mA.
Thank you in advance,
João Rego