Part Number: BQ24296M
Hi.
The datasheet for this PMIC declares several TS limits for the charging mode:

As one can assume, these thresholds must also apply in a charged state (REG08[4:5)=11). And I see from the experiment that they do.
However, in REG08[4:5)=11 states, the hot temperature hysteresis (difference in HFT and TCO limits) seems to disappear. I've done two experiments to check that, in both, there is a multi-turn potentiometer instead of the NTC:
1) REG08[4:5)=11, REG05[7] = 1. PMIC shows <10 mV window between HOT-NORMAL temp states.
2) REG08[4:5)=11, REG05[7] = 0 (disabled termination). PMIC shows a ~120 mV window, as expected from the datasheet values.
Could you confirm that in REG08[4:5)=11 states, there is no HFT-TCO hysteresis window? If so, which one is applied?
Best regards, Vasyl.