Greetings Team,
I have a use case that needs 5 and 3.3 volts on the board to work. I have used the LM61480 design from Webench designer and implemented it. The issue is that I can't seem to operate them simultaneously. I have had good results when only one of them is populated on the board. But when I use them concurrently 3.3V IC shorts internally (inductor pin shorts to GND as soon as the power supply is switched on). Looking forward to your answers.