Hi
I'm Jongyoon.
I'm Currently designing a PFC with UCC28056 and have some questions regarding it.
First, my specifications for I/O is as follows :
Vin (AC) : 198 Vrms ~ 242 Vrms
Pout : 200 W / Vout : 400 V
Here is my questions
1. Selected GFF based on input voltage
: I Understood that GFF is automatically changes when input voltage varies. And I found out that the selected GFF based on the input voltage can be calculated through
Kzc (ZCD resistor divider ratio) and VFF,fall. I want to know that if i am correct about it .
For example, assuming Kzc = 401 (value on the datasheet), since VFF0Fall = 0.331 V
Kzc * VFF0Fall / sqrt(2) = 93.85 Vrms. Therefore I believe when the input voltage goes lower than 93.85 Vrms, GFF0 will be selected for operation.
Am i correct ?
2. Boost inductor design
: So if my understanding in question 1 is correct, is it okay for me to design my boost inductor by following ?
my input voltage range is 198 Vrms ~ 242 Vrms, so i believe that only GFF5 ~ GFF7 values are utilized during operation
LB = (VinRMSMIn ^2 /(110% * Poutmax) )* TONMAX5 *0.5
LB = ((KZC*VFF5FALL)^2 /(110% * Poutmax*2))*TONMAX5 * GFF6 *0.5
and i should use the smaller value
I want to know if i'm correct about it.
I will look forward to your reply
Thanks.