Hello,
I am trying to understand ucc28810 EVM-003 circuit. I have couple questions for this EVM design.
1. Because constant current is reqired to drive LEDs, normally there is a current feedback to maintain the LED drive current. However, I don't see any current sensing feedback circuit at the 3rd stage of the EVM design. How does it work to maintain the constant current?
2. What is the voltage between PFC+ and VBUCK- ( the output of the 2nd stage) is? How does this voltage control (or impact on) LED drive voltage and current at the 3rd?
3. How many isolated LED driving transformer coils does this LLC oscilation circuit can support (It shows 2 in the EVM design) ? How do they influence each other? Specially, when Open Circuit happened, how does the currents in remained LED circuit change? Does the voltage between PFC+ and VBUCK- need to be changed if different number of tranformer coils changes?
4. It looks like D34, R68, R69, C54 and D38 are used for "Open Circuit Protection". As a result, the R69 has to comsume certain amont energy when the circuit opened. This will lower the system efficiency. How much current has to be released through this R69 to keep this circuit work properly? Also please explain more detail for this "Open Circuit Protect" design and related to the LLC oscilation circuit.
Jun