Part Number: TPS92410EVM-002
I have designed a custom TPS92410EVM-002. In there top LED (160V) string is not working.
When the board is powered up it goes to the OVP after a few seconds.
I removed the over voltage protection by connecting the DOV pin of TPS92410P to the GND for the testing purposes.
Changed the R25(RCS) to 60Ohm which limits the avg current to 20mA.(originally it had a 30Ohm resistor and problem is there in both cases)
I checked the bottom and middle LED strings and they are working properly.
I removed the Q3 BJT and gave 14V(across VIN and VS) to the top floating switch from a separate power supply to make sure U1 is always powered up.
I have attached the waveforms captured around the top switch.

waveform across GND and VS1.

waveform across VDS of Q1

waveform across R6.
VGS = 200mV in Q1.
1) What could be the problem of my design?
2) Please explain how the Q1 mosfet should be working in a normal setup?