This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR33630ADDAEVM: How to evaluate LMR33630BDDA(3A/1400kHz) and LMR33640DDDA(4A/1000kHz) using EVM.

Part Number: LMR33630ADDAEVM
Other Parts Discussed in Thread: LMR33630CDDAEVM

Hello guys,

One of my customers is considering using LMR33630BDDA(3A/1400kHz) and LMR33640DDDA(4A/1000kHz) for their new products.

They want to evaluate these devices using TI EVM. But they couldn't find any EVM these devices were mounted on.
At this moment, they have the following question.
Could you please give me your reply?

Q. 
Is there any EVM which LMR33630BDDA/LMR33640DDDA are mounted on?
If the answer is no, Is replacing LMR33630ADDA on LMR33630ADDAEVM with LMR33630BDDA
and replacing LMR33630CDDA on LMR33630CDDAEVM with LMR33640DDDA only way?

It is difficult to solder the thermal pad for them when these devices are replaced.
So it is very helpful if you have any EVM for LMR33630BDDA(3A/1400kHz) and LMR33640DDDA

Your reply would be much appreciated.

Best regards,
Kazuya.