Other Parts Discussed in Thread: UCC25800
Hi
I wanted to go with a multiple secondaries approach, where my previous design is distributed one, I wanted to know that from the highlighted text that
1) Is there any hardware change needed for centralized architecture (except OCP setting), from the attachment I can see that the resonant capacitor role get transferred to primary side capacitors? If hardware change is needed do mention the same in your answer.
2) And If I can manage to design my transformer with leakage inductance equally distributed among all the secondaries then the resonance will be on the secondary side? Since I want to keep the voltage regulation tight. are there any other parameters to take care of to maintain the resonance on the secondary side even with multiple secondaries?
3) Any chances of achieving secondary side resonance with Planar transformer having multiple secondaries?