Other Parts Discussed in Thread: TPS7H6003-SP, UC1875
Greetings,
Could a DC-DC phase-shift bull bridge topology controlled by the following component (UC1875-SP) be used for a step-up/ step-down converter?
Input voltages: 50VDC -200VDC
Output Voltage: 120VDC
Power: 1500W
Or is it only supporting step-up or step-down ( depending on the transformer)?
If it is, could you please recommend a suitable controller for the step-up/step-down application?
Thank you!