Hello Experts,
My customer has question as follows. Would you answer it, please?
[Question]
This is a question regarding the evaluation board circuit diagram provided by your company. Project title [1500V HV AUX Power] Attached is the circuit diagram. Is the pulse transformer T1 for driving Q1 connected to the wrong connection? I think the correct wiring for pin 2 of T1 is VDD, but what do you think? The route for T1's excitation current when Q3 is off is not secured. If I had to say it, it would be T1-3→T1-7→D6→D4→R7//R41→T1-6, but I think that is different from the purpose of D6.
[PMP41031 schematic]
file:///C:/Users/a0385644/Downloads/TIDMBZ3.PDF
Best Regards,
Fujiwara