Other Parts Discussed in Thread: LM25117, LM25148
I am currently developing a CC CV circuit to charge a 28 V battery.
The constant current should be set to 2 A.
I have come across two different Schematics provided by TI Appilcation Notes.
One where the current monitor feeds back directly into feedback and another where it feeds into the Ramp pin.
The main problem is that the input voltage is nominal at 28.8 V.
Would it still be wise to continue with the LM5117?