Part Number: UC2844
Hi expert,
Customer is using UC2844 for Flyback (220Vac/340V-810Vdc input to 24Vdc output, 1A~4A output, 86kHz fsw) use case but met thermal issue. When ambient temperature around 20℃, UC2844 will reach ~90℃ with thermal risk, SCH and partial PCB as below:


Could you help give some comments and suggestions on this? Thanks!
Joyce