Other Parts Discussed in Thread: UCC27524
Hello Team,
We have designed the 1600W PFC design using the UCC28180. We are using the same chip for the different designs like 450W, 600W & 900W works well. But in the higher power 1750W, we are facing the output voltage regulation issues. The problem starts once we load the PFC more than >600W at input of 230VAC, the output voltage will be fluctuating from 390V to 420V, and PF is coming down to <0.70. Please help me out of this problem...
Updated Values:
1. ICOMP: 1500pF
2. FREQ: 17.4K 120KHz
3. ISENSE: R 220E & C 1nF & Diode BAS21
4. VSENSE: Top R 996K & Botto R 13K & C 1nF
5. VCOMP: Series R 16K & Series C 10uF & Parallel C 0.47uF
6. Gate Driver : UCC27524DGN & Dual Mosfets: TK110N65Z,S1F
7. Diode: C3D16065A
8. Series Diode: 1N5408
7. Output VBUS Cap: 470uF x 3
8. Input Cap: 680nF
9. Inductance: 264uH PQ5050
Kind Regards,
Nishanth M