This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2991: Inquiry about DC/DC converter recommendation that supports negative voltage

Guru 10860 points
Part Number: LM2991
Other Parts Discussed in Thread: TPS40210, TPS61086, TPS61170, TPS61175

Hello,

My customer is looking for DC/DC products that can be used for the following conditions.

  - VIN = -15V, VOUT = -6V, IOUT = about 300mA(typ) : Best if it can support up to 1A

They prefer DC/DC products over LDO to reduce heat generation. Additionally, due to space constraints, the smallest package size is required (less than 4 mm in height).

Please recommend which of TI's DC/DC products best suits the customer's requirements.

Thank you.

JH