Other Parts Discussed in Thread: REG710-5, REG710-3, TPS61299
Hello,
I'd like to use the REG71050 for boosting an input that ranges between 1.8 V and 3 V. The dataheet table for input operating voltages, table 7.3, indicates that the device should operate down to 1.8V. But all the efficiency graphs for REG71050 extend no further than 2.7 V, in each case showing only the range common to both REG71050 and REG710-5. Do you have the data for REG71050 between 1.8V and 2.7V available for customers?
(Also, as a side note, I think a copy-paste error messed up your device label in Fig 11. From context, it appears that TI meant for it to be REG710-3 not REG710-3.3, its neighbor.)
Best,
Janet Stillman