This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5010: short circuit destroys device

Part Number: LM5010
Other Parts Discussed in Thread: TPSM365R6

Hey team, 

can you please help:

We continue to use the LM5010MH/NOPB HTSSOP14 regulator in a redesign.

If this is short-circuited at the output p24V to GND and the short-circuit is removed again, we destroy the regulator.

In the previous design this was possible without any problems, after the short circuit the controller started up again. The layout and component values are identical in the redesign. (Minimal manufacturing-related deviations in the layer structure)

Our assumption is that in the event of a short circuit via C121 and C120, we generate a negative voltage pulse at the feedback, which destroys the internal protective diode at the feedback.

The controller is also very susceptible to ESD.

  1. Does TI have any information on the phenomena described?
  2. How long will the regulator still be available, as a newer version TPSM365R6 is advertised on the homepage, which unfortunately is not footprint identical?

thanks 

Jan