Hi,
There are 2 totem pole topologies.
1. interleave totem pole (used in TIDm-02013)
2. Totem-Pole Bridgeless PFC (Diode Rectification)
My question is can we use Totem-Pole Bridgeless PFC (Diode Rectification) for bidirectional OBC?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
There are 2 totem pole topologies.
1. interleave totem pole (used in TIDm-02013)
2. Totem-Pole Bridgeless PFC (Diode Rectification)
My question is can we use Totem-Pole Bridgeless PFC (Diode Rectification) for bidirectional OBC?
BL TotemPole PFCs(TTPLPFC) can operate in both directions. Diode rectifiers can support PFC action in a BL TTPLPFC. This is because the diodes will be forward biased in this mode.
To answer your question please consider the power flow when in reverse conduction. Figure 4 of the following IEEE paper shows the power flow in a V2G application. The synchronous rectifier FETs are reverse biased in this case. If you replace these with diodes the current will be blocked, and rectification cannot occur.
https://ieeexplore.ieee.org/stamp/stamp.jsp?tp=&arnumber=7467909&tag=1
Regards,
Cody
Thanks Cody.
If you can share the IEEE screenshot here which you are referring to.
Alihussain,
I do not believe I can share that directly if it is not in the public domain. It shows current flowing in the reverse direction across the switch. This must happen as power is leaving the battery and going to a load/grid in a V2G application.